Herramientas para el montaje de rodamientos

Montaje de rodamientos en frío

El fallo prematuro puede ocasionarse como consecuencia del daño producido al montar un rodamiento incorrectamente.

Los problemas típicos que pueden causar fallos prematuros son:

  • Daños causados durante el procedimiento de montaje
  • Ejes y soportes incorrectos, es decir, ajustes demasiado fuertes o demasiado flojos
  • Las tuercas de retención se aflojan durante el funcionamiento
  • Ejes y soportes arañados y dañados
  • Rodamientos montados incorrectamente

Herramientas para el montaje de rodamientos

Interference fits: cylindrical shafts

Shaft interference fit
Shaft interference fit
Housing interference fit
Housing interference fit
Most bearings are fitted to their shaft or housing with one component having an interference fit. For determining the correct fit, refer to the SKF General Catalogue, the SKF Maintenance Handbook or consult an SKF application engineer.

Incorrect mounting
When bearings are mounted cold, care must be taken to make sure the drive-up forces are applied to the ring with the interference fit. Damage and a resulting bearing failure can occur if the mounting force is transmitted through the rolling elements causing damage to the raceways (fig 1)

Correct mounting
The correct way to minimise raceway damage is to use specifically designed tools from SKF, such as the Bearing fitting tool kits and Combi kits. These tools allow drive-up forces to be applied effectively and evenly to the component with the interference fit avoiding raceway damage (fig 2)

Interference fits: tapered shafts

Bearings mounted on tapered seatings achieve their interference fit by being driven up the tapered shaft. Care should be taken to make sure the bearing is not driven up too far, as all the internal clearance may be removed and damage to the bearing is possible. 

Spherical roller bearings
Method: Correct adjustment of spherical roller bearings is determined by measuring the residual internal clearance in the bearing or by the amount of axial drive-up. Details of the required reduction of clearance and axial drive-up can be obtained from tables published in the SKF General Catalogue. For larger size bearings, it is generally recommended to consider using a tapered seating to facilitate easy mounting and dismounting.

Self aligning ball bearings
Method: Adjustment of double row, self-aligning ball bearings is more difficult to achieve than spherical roller bearings because the feeler gauge method cannot be used. A very effective method to mount this type of bearing correctly is to use the SKF TMHN 7 lock nut spanner set.

Incorrectly mounted: Bearing driven up too far and all clearance removed; damage possible (fig 3)

Correctly mounted: Bearing driven up the correct distance and the right clearance is achieved (fig 4)

SKF logo