SF 70-H


On February 24th the new Scuderia Ferrari F1 single seater (SF70-H) has been officially presented in Maranello.

The 63rd single-seater designed and built by Scuderia Ferrari to take part in the Formula 1 World Championship is born out of a regulation change that is without precedent in this category of motor sport. Generally, in the past, regulations went in the direction of slowing down the cars. However, this year, the rule changes go in the opposite direction, meaning the cars have more aerodynamic downforce and more mechanical grip.

Stechnical characteristics of the new car:

  • 1600 cc capacity
  • Single Turbo supercharging
  • MGU-H max. revs: 125.000 RPM
  • 728kg weight with water, lubricant and driver
  • 8 + R gears
  • Carbon-fibre chassis
  • 13“ OZ wheels
SKF logo