SKF Housing Select

Facts
Language: English
Format: Web application
Product platform: Bearing, units and housings
SKF Housing Select

The program will search for SKF bearing housings according to the criteria that have been specified. Selecting a housing from the result list will show the specifications for the housing with the components that are specified in the search criteria.

If a bearing with tapered bore is specified, the specifications that are necessary for proper mounting of the bearing will be shown when checking the appropriate radio button preceeding the bearing designation.

The housings that are considered for the search are
  • split plummer/pillow block housings in the series SNL 2, 3, 5 and 6
  • split plummer/pillow block housings in the series large SNL 30, 31 and 32 
  • split plummer/pillow block housings in the series SONL 
  • split plummer/pillow block housings in the series SAF 
  • one-piece plummer/pillow block housings in the series TVN 
  • flanged housings in the series 7225(00)
Enter promo code
SKF logo