Load carrying capacity

PD two-bearing housings are intended for loads acting perpendicularly toward the support surface. If the housing is supported over its four feet and the loads are purely perpendicular, loads are limited only by the bearings.
Housings in the PDN series that have bearings preloaded with a wave spring washer accommodate axial loads in one direction only.
SKF logo