Verify the lubrication condition, consider EP/AW additives
The lubrication condition κ, is evaluated by using the base oil viscosity as described in
Lubrication condition – the viscosity ratio, κ. In the lubrication condition domain defined by κ below 1, EP/AW additives are recommended.
EP/AW additives of the sulphur-phosphorus type, which are the most commonly used today, may also have a negative influence on the fatigue life of the bearings. This is because in the presence of humidity, which can never be completely avoided, sulphur and phosphorus acids are produced which induce a more aggressive chemical process at the rolling contact. This effect increases with temperature and, for temperatures above 80 °C
(175 °F), a lubricant with EP/AW additives should only be used after careful testing. SKF greases have been tested and can be used above 80 °C
(175 °F) until the HTPL is reached.
Low speeds
Bearings that operate at very low to low speeds (table 2) under heavy loads should be lubricated with a grease that has a high viscosity base oil and contains EP additives. The thickener should contribute to the surface separation. Sufficient oil bleeding should assure oil replenishment during operation.
Solid additives, such as graphite or molybdenum disulfide (MoS2), should be considered for a speed factor ndm < 20 000 mm/min. SKF LGEV2 is successfully used up to ndm = 80 000.
Heavy and very heavy bearing loads
For bearings subjected to a load ratio C/P < 4, the calculated relubrication interval may be so short that it dictates the use of continuous relubrication or oil lubrication.
Miscibility with other greases
If it becomes necessary to change from one grease type to another, consider the miscibility of the greases and their ability to be mixed without adverse effects (
table 4 and
table 5). If incompatible greases are mixed, the consistency of the grease mix can change dramatically such that bearing damage due to severe leakage could result. Note that PTFE-thickened greases are not compatible with other grease types.
Miscibility with preservation oils
The preservative oils with which SKF bearings are treated are compatible with the majority of lubricating greases, with the exception of synthetic fluorinated oil based greases using a PTFE thickener, for example, SKF LGET 2 grease. For PTFE-thickened greases, the bearing preservatives must be removed before applying the grease. White spirit is recommended as a solvent. Make sure all remnants of solvent have evaporated and then immediately apply the grease.