Climate strategy

SKF’s climate strategy is focusing on CO2, which is concluded to be the most significant greenhouse gas produced as a result of our business activities. It is based on the BeyondZero thinking model to reduce the negative and increase the positive. 
 
Baes on a number of life cycle assessments of our products and solutions we have clearly found that the use phase is – by far – where we can make the most significant contribution to climate change mitigation. However, in line with BeyondZero, we also believe that it is our responsibility to use our combined knowledge, experience, influence and creativity to minimize the negative environmental impact deriving from our operations long the entire value chain.
 
SKF’s climate strategy 2012-2016 is focusing on four areas, where the carbon intensity is relatively high and SKF has the possibility to drive real, positive change. We have set ourselves touch targets and we can show solid performance over time: 

Metas da mudança climática através da cadeia de valor

SKF’s climate strategy 2012-2016 focused on four areas, here’s what we have achieved...



The targets focused in four areas where the carbon intensity is relatively high and SKF has the possibility to drive real, positive change. We set ourselves tough targets and we can show solid performance over time:


On our own manufacturing, SKF said we would decrease energy use (this closely correlates with CO2 emissions) to 5% less than our 2006 level. By the end of 2016 we were at 14% reduction. During this time SKF’s business grew by over 35%.  
We also targeted to reduce energy directly associated to production output by 5% every year. This has been trickier since the production rate has differed significantly over the years. We managed to make this from 2015-2016.
What’s next?

On goods transportation SKF said that we would reduce the CO2 intensity (CO2 emissions per tonne-kilometre) by 30% between 2012 and 2016. This was achieved by 2016 when the annual emissions were reduced by 31%.
What’s next?


On raw materials and purchased goods SKF said that all major suppliers that are energy intensive shall be certified to ISO 50001 energy management (as is SKF). By the end of 2016, 84% are certified and the rest are working towards certification.
What next?

On customer solutions SKF said we would grow the revenue from the SKF BeyondZero portfolio from SEK 2.5 bn in 2011 to SEK 10 bn by year-end 2016. By the end of 2015, SKF BeyondZero customer solutions revenues amounted to nearly SEK 7 bn.

We saw already in 2013 that 10 billion was going to be too ambitious but chose not to change the target. One very positive sign is the 2015 to 2016 increase which is mostly related to organic sales increase. SKF will continue to measure and report both revenues and avoided emissions from the BeyondZero customer solutions. The growth will be supported by inclusions of new solutions as well as sales growth of existing ones.

Whats next?

SKF logo