SKF to present its marine portfolio at Nor-Shipping

SKF and SKF Blohm + Voss Industries will be presenting their combined marine product portfolio at the Nor-Shipping trade fair, stand E 03-19. The event takes place between 2-5 June in the Norges Varemesse exhibition halls outside Oslo, Norway.

With the acquisition of SKF and Blohm + Voss Industries, customers can look forward to benefiting from an expanded and perfectly coordinated marine product and services portfolio. A product- and service portfolio where customers will be able to profit from both companies´ experience and knowledge: twice the experience, reliability and marine know-how.

The theme “Twice the power” will be the red thread through the exhibition. One example of this is the impressive thruster exhibition model, which will be set up at Nor-Shipping. Visitors can see for themselves the full range of associated products and services with the help of this two metre-plus replica of a thruster. Everything from the bearings, the gear coupling and lubrication system to the SIMPLEX-COMPACT seal and the propeller sleeve will be displayed. Also on show here are supplementary services such as condition monitoring solutions and alignment services.

Besides these attractions, visitors can see a SIMPLEX-COMPACT sterntube seal, product presentations of the commercial steering engine and BlueMon, an environmental monitoring system for measuring and recording emissions, and solutions in the fields of alignment services, condition monitoring and coupling systems.

Furthermore, the marine team is pleased to have Reed Olsen & Schytz as its direct stand neighbor. The Norwegian ship chandler and marine supplier is the exclusive sales agent for SKF Blohm + Voss Industries products on the Norwegian market and a long-term partner. 

More information about the trade fair can be found on the official Nor-Shipping website at: www.messe.no/nor-shipping
SKF logo