Business Care

确保财务状况良好, 为股东实现投资回报。

SKF China obeys the ten principles of the United Nations Global Compact and is committed to applying its knowledge to engineering solutions to help clients improve technologies and save energy.

Compared with traditional bearings, SKF energy efficiency tapered roller bearings and cylindrical roller bearings perform far above the ISO standard requirement by reducing fricton by at least 30% and saving energy directly for clients.

While focusing on energy efficiency, SKF actively develops new technologies and industry solutions. For instance, jointly establishing the repair centre with Baosteel is an example of SKF’s pioneering work in environmental protection: the creative SKF ConRo can help clients not only in improving production efficiency and cutting costs, but in reducing damage to the environment caused by various steps in the production process.

More than that, based on business care, SKF has launched a brand-new concept “Life Cycle Management” with nine major unctions to maximize equipment productivity and lower costs.

助力设备 发挥最佳运作

SKF Life Cycle Management, a new concept SKF has introduced based on business care, can maximise the efficiency of equipment production and minimise the total cost of every stage, from standardised design to operation and maintenance. Whether you are in charge of engineering, maintenance, stability, or operations, SKF Life Cycle Management fully supports you in:

1. Optimising design
2. Reducing the time-to-market and
    production cost of products
3. Improving efficiency of energy and resources
4. Improving reliability
5. Extending the service life of equipment
6. Improving productivity
7. Improving safety
8. Minimising maintenance
9. Lowering total cost
SKF logo