SKF (Dalian) Bearing and Precision Technologies Co., Ltd. Large Size Bearing Factory

SKF (Dalian) Bearing and Precision Technologies Co., Ltd., located in Dalian, China, is the largest bearing manufacturing site of SKF in China. Its main businesses include the production and rebuilding of high performance precision bearings, relevant technical consultancy and aftersale services as well as import and export of products and technology.

SKF Dalian has two factories for large size and medium size bearings repectively. They were put into production in2006 and2011,with totally more than 600employees. Up to now, SKF (Dalian) Bearing and Precision Technologies Co., Ltd. has confirmed an investment ofabout 1.5billion RMB.
SKF Dalian large size bearing factory covers a total area of80,459square meters. With 11production lines, it is able to manufactureSKF Explorerspherical roller bearings, cylindrical roller bearings, deep groove ball bearings, angular contact bearings, spherical roller thrust bearings, slewing bearings and"Nautilus"bearings, etc. with maximum OD of 4 meters. The applications of its products include renewable energy, engineering machinery, metal, mining and mineral processing as well as cement, paper, material handling, industrial motor and transmission, etc.
SKF Dalian was awarded many trophies including "Dalian Best Employer" in two consecutive years, DalianAAA-grade Employee Trustworthy Enterprise, Dalian Model Harmonious Labor Relationship Enterprise and -AA-grade Labor Security Laws and Regulations Compliance Integrity Unit.



Address and contact:

Address:No. 87, Huai He Zhong Road Dalian Economic & Technological Development Area Liaoning Province
Tel:+86 411 3921 9083
Fax:+86 411 3921 9001

SKF logo