SKF (Shanghai) Bearings Co. Ltd.


SKF (Shanghai) Bearings Co. Ltd., located in Jinqiao of Pudong district and established in 2001, became a wholly-owned subsidiary of SKF since2007.

It is a automated factory specilized in production of deep groove ball bearings for automobile ranging from 32mm to62mm OD and11 basic versions withmore than 400varients.

The company has been approved by the following quality system certifications:


•2005 : ISO 14001
  OHSAS 18001

  2008:ISO/TS 16949-2002

  2009:ISO 14001-2004
  OHSAS 18001-2007

Address and contact:

Address: No.999 Xin Jin Qiao Road, Pudong, Shanghai
Zip code: 201206
Tel: (021) 5032 5655
Fax: (021) 5031 1412 
SKF logo