Ordering information

For SE housings in the 2, 3, 5 and 6 series, each of the following items must be ordered separately:
  • housing
  • seals
  • end cover
  • locating rings
  • bearing
  • adapter sleeve

Order example

Two plummer block housings with four-lip seals are required for a 22212 EK spherical roller bearing on an H 312 adapter sleeve and a C 2212 KTN9 CARB toroidal roller bearing on an H 312 E adapter sleeve. One housing will accommodate the non-locating bearing at the end of the shaft. The other housing will accommodate the locating bearing and a through shaft.
The following items should be ordered (in addition to the bearings and adapter sleeves):
  • 2 housings SE 512-610
  • 2 four-lip seal packs TSN 512 L (each pack contains two seals)
  • 1 end cover ASNH 512-610
  • 4 locating rings FRB 10/110
SKF logo