Reduce downtime with remanufactured bearings

Railway
In high speed rail, there is no room for quick fixes. On the contrary. The pressure on railways to work more efficiently, safely and productively while reducing costs is higher than ever.

SKF service manager Stewart McLellan and SKF remanufacturing teams around the world offer a solution. They can have wheelset bearings correctly disassembled, washed, inspected, measured, greased and reassembled with new components. The bearings can also be upgraded to a higher standard. After this, the bearings are quickly returned to the customer, and the vehicle is right back on track.

The bottom line? Minimized downtime, optimized assets, and reduced environmental impact. It’s another great example of knowledge engineering at work.

SKF engineers tell how they develop industry-specific solutions

SKF logo