Youth empowerment in Kenya

In 2015, in collaboration with the local SWHAP (Swedish Workplace HIV/Aids Programme), SKF Kenya has initiated successful workshop training for children and young adults on issues confronting young people today, such as anxiety, self-esteem, sexuality, alcohol and substance awareness, excessive use of internet, friendships and peer pressure. Economic development is moving rapidly in sub-Saharan Africa, and along with this, new needs and challenges emerge. The goal is to help these young people to gain useful life skills which help them to face up to these challenges and succeed.

SKF logo