SKF超越零组合

以零为目标是优良。 但超越零更是精益求精。

SKF超越零组合是从客户的角度出发而开发的。 它包括来自SKF的产品和解决方案,它们在以下领域为客户带来显著的环境效益:
  • 帮助保护大气平衡。
  • 提高有效和环保的土地资源使用。
  • 避免向水体排放。


超越零组合中包含的一些产品和服务介绍如下:

行业分类

航空航天

农业和建筑

轿车和轻型卡车


电机和发电机

流体机械

食品和饮料
机床 
医疗与保健 
冶金

纸浆和造纸 
铁路
服务 
卡车、挂车和公共汽车 
两轮和三轮车 
  • 入选标准
    Solutions within the SKF BeyondZero portfolio must provide significant environmental benefits without serious environmental trade-offs, from a life cycle perspective. They need to address one or more defined environmental challenges, such as, climate change, natural resource use and the avoidance of various types of environmental contamination.

    This can be done in one of two ways:
    • The product or solution can be “Designed for environment”; it provides environmental benefits in its own right through some inherent characteristics (such as low friction or low weight),
    • or it can be “Applied for environment”; the product or solution helps to improve the environmental performance of the system (customer application) in which it is applied.

    SKFs complete business within the renewable energy industry as well as SKF’s emerging business in the full electric vehicle industry are included in the SKF BeyondZero portfolio under the “Applied for environment” category. These industries are included because it is widely acknowledged that they are technologically critical to reducing fossil fuel use and therefore addressing climate change.

    The benefits are derived from a comparison of the environmental performance of SKFs solution to that of a defined baseline.
  • 管理
  • 方法
SKF logo