Cookies en el sitio web de SKF

Utilizamos cookies para garantizar que le brindamos la mejor experiencia posible en nuestros sitios y aplicaciones web. Si continúa navegando sin cambiar la configuración de su navegador, supondremos que acepta recibir cookies. No obstante, puede cambiar la configuración de cookies de su navegador en cualquier momento.

Oil lubrication

Oil is generally used to lubricate rolling bearings when:
  • high speeds or operating temperatures preclude the use of grease
  • excessive heat has to be removed from the bearing position
  • adjacent components (gears etc.) are lubricated with oil
To extend bearing service life, all methods of bearing lubrication that use clean oil are acceptable. These include:
  • the circulating oil lubrication method
  • the oil jet method
  • the oil-air method
When using the circulating oil or oil-air method, adequately dimensioned ducts should be provided so that oil flowing from the bearing can leave the arrangement.
SKF logo