Cookies en el sitio web de SKF

Utilizamos cookies para garantizar que le brindamos la mejor experiencia posible en nuestros sitios y aplicaciones web. Si continúa navegando sin cambiar la configuración de su navegador, supondremos que acepta recibir cookies. No obstante, puede cambiar la configuración de cookies de su navegador en cualquier momento.

Vibration behaviour of the application

In many applications bearing stiffness is of the same order as the stiffness of the surrounding structure. This opens the possibility to reduce vibrations of the application by properly choosing the bearing (including preload and clearance) and its arrangement in the application. There are three ways to reduce vibration:
  • Remove the critical excitation vibration from the application.
  • Dampen the critical excitation vibration between excitant component and resonant components.
  • Change the stiffness of the structure to change the critical frequency.
SKF logo