Speed control

In many cases it is important to know punctually the rotational speed of the motor with the best accuracy. Then the best possible solution is to have the speed sensor mounted on the same shaft of which we want to measure the rotational speed and even better is to have the sensor integrated in the bearing that supports that shaft.

Solutions

SKF logo