Hub bearing units

Smaller houses and competing washing machines producers that are increasing the load carrying capacity of their machines request the application of new technologies derived from the automotive field. SKF has developed integrated units to support the drum with the following advantages:

  • Higher stiffness
  • More compactness
  • Higher carrying capacity
  • Water exclusion

The unit is made of a bearing arrangement lubricated for life and seals developed for the mud and slurry test.

SKF logo