Simplify with SKF Marine

Following the acquisition of Blohm + Voss Industries by the SKF Group in 2013, the marine segment communicated this through campaigns where both logotypes were visible. Now, around two years later, SKF Blohm + Voss Industries will become SKF Marine from the beginning of September 2015. This step will further strengthen the marine industrial part of SKF and create a clear profile for customers.

Simplify with SKF Marine will be the concept towards the market, as we would like to show the full portfolio of high quality components, products and services we can provide in a simplified way. We know that the business is complex enough. From now on, when you’re ready to simplify, the name is SKF Marine.
SKF logo