SKF and Ducati Corse

Ducati Desmosedici 2017 + logos
Ducati Desmosedici MotoGP17
Ducati is a company with a unique philosophy, inspired by the extremely close bond with its racing activities. This bond has led to the development of a profound synergy between the evolution of its competition motorcycles and its consumer products. Racing is an integral part of this synergistic evolution, leading to the quality and reliability of both its racing and consumer applications.

Founded in 1926, Ducati has been producing sport-inspired motorcycles since 1946. Today, their motorcycles are characterized by performance engines with Desmodromic valve actuation, innovative design and avant-garde technology. Covering several market segments, Ducati's range of motorcycles is divided into model families which include: Diavel, Hypermotard, Monster, Multistrada, Scrambler, Streetfighter and Superbike. These authentic icons of “made in Italy”, together with an extensive range of associated accessories and technical and lifestyle apparel, are distributed in over 80 countries around the world, with concentration on the European, North American and Asia-Pacific markets. Ducati competes in both the World Superbike and MotoGP World Championships. In Superbike Ducati has won 17 Manufacturers' titles and 14 Riders' titles and in 2011 passed the historic milestone of 300 race victories. Ducati have participated in MotoGP since 2003, winning both the Manufacturers' and Riders' titles in 2007.
SKF logo