Racing

From the beginning of the quads with wooden wheels to the rise of in-line speed skating, races are the places to test new equipment and technologies. There are several big events like Roller World cup, national cups and championships, and many more everywhere in the world. There are many race types and places:

  • Races on track - indoor or outdoor - from 300 m to 10000 m
  • Marathons on roads - 42 km or more
  • Downhill
  • Urban races

Solutions

SKF logo