Microlog idler sound monitor

Facts
Date: 2013
Language: English
Webinar screenshot

A demonstration

In many industries, conveyors are an important part of a material handling system, especially in mining and cement industries. Failure of an idler can lead to belt damage, expensive downtime and lost production. The SKF Idler Sound Monitor Kit was developed for early detection of faults in conveyor support and return idlers. 

This session demonstrates the use of acoustic enveloping technology in the SKF Idler Sound Monitor to distinguish between the sounds of a good idler and a faulty one. 


Enter promo code
SKF logo