SKF BeyondZero portfolio

Targeting zero is good. Going beyond zero is better.

The SKF BeyondZero portfolio was created from a customer perspective. It includes products and solutions from SKF which bring significant environmental benefits to our customers in one of the following areas:
  • Help preserve the balance of the atmosphere.
  • Promote efficient and responsible use of land resources.
  • Avoid discharges into water.


Some of the products and services included in the BeyondZero portfolio are presented below:

Inclusions by industry

Aerospace

Agriculture and Construction

Cars and light trucks


Electric motors and generators

Fluid Machinery

Food and beverage
Machine tool 
Medical and health care 
Metals  

Pulp and paper 
Railways
Services 
Trucks trailers and buses 
Two-threewheelers 
  • Critieria for inclusion
    Solutions within the SKF BeyondZero portfolio must provide significant environmental benefits without serious environmental trade-offs, from a life cycle perspective. They need to address one or more defined environmental challenges, such as, climate change, natural resource use and the avoidance of various types of environmental contamination.

    This can be done in one of two ways:
    • The product or solution can be “Designed for environment”; it provides environmental benefits in its own right through some inherent characteristics (such as low friction or low weight),
    • or it can be “Applied for environment”; the product or solution helps to improve the environmental performance of the system (customer application) in which it is applied.

    SKFs complete business within the renewable energy industry as well as SKF’s emerging business in the full electric vehicle industry are included in the SKF BeyondZero portfolio under the “Applied for environment” category. These industries are included because it is widely acknowledged that they are technologically critical to reducing fossil fuel use and therefore addressing climate change.

    The benefits are derived from a comparison of the environmental performance of SKFs solution to that of a defined baseline.
  • Governance
  • Methodology
SKF logo