Angular contact ball bearings

Angular contact ball bearings have raceways in the inner and outer rings that are displaced relative to each other in the direction of the bearing axis. This means that they are designed to accommodate combined loads, i.e. simultaneously acting radial and axial loads.
The axial load carrying capacity of angular contact ball bearings increases with increasing contact angle. The contact angle is defined as the angle between the line joining the points of contact of the ball and the raceways in the radial plane, along which the load is transmitted from one raceway to another, and a line perpendicular to the bearing axis (fig. 1).
SKF angular contact ball bearings are manufactured in a wide variety of designs and sizes. The most commonly used designs are:
  • single row angular contact ball bearings (fig. 2)
  • double row angular contact ball bearings (fig. 3)
  • four-point contact ball bearings (fig. 4)

Designs and variants

SKF logo