Misalignment

Angular contact thrust ball bearings cannot tolerate any misalignment of the shaft with respect to the housing or any angular misalignment of the support surfaces on the shaft and in the housing.
SKF logo