Bearing handling

It is generally a good idea to use gloves as well as carrying and lifting tools, which have been specially designed for mounting and dismounting bearings. This will save not only time and money but the work will also be less tiring, less risky and less injurious to health.
For these reasons, the use of heat and oil resistant gloves is recommended when handling hot or oily bearings. These gloves should have a durable outside and a soft non-allergenic inside, as, for example, SKF TMBA gloves.
Heated and/or larger or heavier bearings often cause problems because they cannot be handled in a safe and efficient manner by one or two persons. Satisfactory arrangements for carrying and lifting these bearings can be made on site in a workshop. The bearing handling tool TMMH from SKF is one such arrangement, which solves most of the problems and facilitates handling, mounting and dismounting bearings on shafts.
If large, heavy bearings are to be moved or held in position using lifting tackle, they should not be suspended at a single point, but a steel band or fabric belt should be used (fig 1). A spring between the hook of the lifting tackle and the belt facilitates positioning the bearing when it is to be pushed onto a shaft.
To ease lifting, large bearings can be provided on request with threaded holes in the ring side faces to accommodate eye bolts. The hole size is limited by the ring thickness. It is therefore only permissible to lift the bearing itself or the individual ring by the bolts. Make also sure that the eye bolts are only subjected to load in the direction of the shank axis (fig 2). If the load is to be applied at an angle, suitable adjustable attachments are required.
When mounting a large housing over a bearing that is already in position on a shaft it is advisable to provide three-point suspension for the housing, and for the length of one sling to be adjustable. This enables the housing bore to be exactly aligned with the bearing.
SKF logo