Sealing solutions

The factors that influence the choice of the most appropriate sealing solution include:
  • the circumferential speed of the seal counterface
  • the seal friction and the resulting temperature increase
  • the environmental influences, e.g. moisture, dust or coarse contaminants
  • the requirements regarding effectiveness
For the different Insert bearings sealing solutions and their characteristics, refer to Sealing solutions.
SKF logo