Components and materials
A typical rolling bearing consists of the following components (fig. 1):
- an inner ring
- an outer ring
- balls or rollers, as rolling elements
- a cage
SKF supplies several bearing types capped with a seal or shield on one or both sides. Bearings capped on both sides are factory-filled with grease. They provide an economic and space-saving solution compared to external sealing.