Misalignment

Double row cylindrical roller bearings can only tolerate very slight angular misalignments of the inner ring with respect to the outer ring. For bearing arrangements, e.g. in rolling mill straightening machines, where misalignment of the inner ring in relation to the outer ring cannot be avoided, SKF can supply bearings having radial internal clearance which is adapted to the application and which is different for the two rows of rollers. In this way the load will be equally divided between the two roller rows under misaligned conditions.
SKF logo