Design considerations

Abutment dimensions

Abutment dimensions should fulfill the following:

  • Support surfaces on shafts and in housings should be at right angles to the shaft or housing axis and should provide uninterrupted support over the entire washer face.
  • The abutment diameter on the shaft should be ≤ Ea and in the housing ≥ Eb.
    Values for Ea and Eb (→ product table) take the movement and position of the roller set into consideration.
  • Shafts and housings should be manufactured to suitable tolerance classes (table 1).
    to provide satisfactory radial guidance for the individual thrust bearing components
    • Housing centred washers → radial space between the shaft and washer bore required
    • Shaft centred washers → radial space between the washer and the housing bore required

Needle roller and cage thrust assemblies in the AXW series are generally combined with drawn cup needle roller bearings (fig. 1) or needle roller bearings with machined rings (fig. 2). The same housing tolerance must be selected for the centring flange as for the radial bearing.

Needle roller and cage thrust assemblies are generally shaft centred, to reduce the circumferential speed at which the cage slides against the guiding surface. This is particularly important for higher-speed applications. The guiding surface should be ground.

Raceways on shafts and in housings

  • should have the same hardness, surface finish and axial run-out as a bearing washer, if the load carrying capacity of a needle roller and cage thrust assembly is to be fully exploited
  • should be designed using the dimensions Ea and Eb (→ product table), which take radial displacement of the roller set into consideration

For additional information, refer to Raceways on shafts and in housings.

SKF logo