Tolerance symbols

The tolerance symbols used in the tolerance table are listed together with their definitions in the table Tolerance symbols which is also accessible from all tolerance tables.
SKF logo