SKF Static Motor Analyzer Baker AWA-IV Family

Automated surge/step-voltage/resistance analyzer for testing static (or off-line) motors

Baker AWA-IV
Baker AWA-IV
The SKF Static Motor Analyzer – Baker AWA-IV series of electric motor analyzers are fully-automated, user-programmable instruments that deliver reliable testing of motors with repeatable results, regardless of user. These easy-to-use instruments perform a wide range of electrical tests, including surge, DC hipot, step voltage, continuous ramp, meg-Ohm and winding resistance tests. Models include the Baker AWA-IV 12 kV, Baker AWA-IV 12 kV HO, Baker AWA-IV 6 kV, Baker AWA-IV 4 kV, and Baker AWA-IV 2 kV.
  • Improved testing capabilities from previous Baker AWA versions: continuous ramped step-voltage, enhanced reference surge waveform, improved PI/DA test, improved DC hipot, improved resistance test, more sensitive surge test
  • As of June 2014, the Baker AWA-IV uses the Microsoft Windows 7 Embedded operating system, which enables faster boot-ups, smoother operation, wider printer compatibility, and both wired and wireless networking (wireless only with the optional USB wireless network adapter).

For more information, contact your local authorized dealer of SKF electric motor test and monitoring solutions. You can also send an email to salesemcm@skf.com, or in the United States, call +1 970 282 1200.

Designed for fast, reliable, automated testing

The SKF Static Motor Analyzer - Baker AWA-IV is designed to perform automated sequences of a user-selected array of motor insulation tests. The analyzer's embedded computer conducts the tests, stores the results and continuously monitors voltage levels while testing. If the computer detects a weakness in the insulation during a given test, the test is interrupted, the operator is alerted and all test parameters at the time of the interruption are reported. This instrument performs this automated operation in microseconds, and with a higher degree of precision and safety than can be achieved through manual test methods.

Pre-programmed in the office and implemented in the field

The Baker AWA-IV is the only high-voltage tester that can be programmed to perform a specific set of insulation tests by a user prior to being in the field, then used as programmed in the field. A user's work orders or routes often define which motors to test, the order of execution and parameters for each test, such as voltages, duration and pass-fail limits. Operators can program the unit to conduct tests in the field simply by connecting to the analyzer. This allows users to minimize time and effort involved with repeat maintenance test sequences performed manually, and improves reliability of testing procedures.

Save testing results

When testing is complete, results can be saved as part of each motor's permanent test record. This type of documentation is critical to successful reliability programmes. With the AWAIV, test results are collected, stored, recalled and managed using a standard Microsoft Access® relational database format. The Baker AWA-IV produces .rtf type test data files, so a variety of desktop computer word processing software programmes can be used. These database files make it easy to transfer information to common maintenance management software or other database tools. MS Access® is ODBC compliant.

Incorporates advanced inter-turn capabilities in a field portable instrument

Computer control and waveform monitoring are enhancements above manually controlled instruments. As with the DC HiPot test, the Baker AWA-IV begins surge generation at low voltage. Each pulse applied to the winding is digitized and the resultant waveform is compared to previous waveforms to detect any signs of turn-to-turn weaknesses. Comparison is done by the patented Pulse to Pulse Error Area Ration (PP-EAR) technique. This method is sensitive to less than a one percent variance between coils. In addition, shorts among windings in parallel can be located, something that was never possible before by visually comparing waveforms. With the Baker AWA-IV, fewer pulses are applied to the winding, reducing the power required to perform the surge test. Since each and every pulse is analyzed, it becomes the new reference waveform as test voltage is increased up to the specific withstand level. If no turn-to-turn weakness is detected, the final pulse waveform is stored as the reference waveform for all subsequent tests.
SKF logo