Water pump bearing seals

Water pump bearing seals are specifically designed for water pump applications.

The water pump is the heart of the automotive cooling system, typically a belt-driven centrifugal pump. The pump circulates coolant throughout the system while the engine is running. If the drive belt fails, the water pump will not function. It is one of the reasons it’s so important to always check the status of the belt during maintenance.

The water pump uses centrifugal force to send coolant to the outside while it spins, drawing coolant from the centre continuously. The pump inlet is located close to the centre so that coolant returning from the radiator strikes the pump vanes, which then fling the coolant to the outside of the pump to enter the engine. Coolant leaving the pump first flows through the engine block and cylinder head, then through the radiator and finally back to the pump.

Features
  • Variety of lip designs: double lip; R-Safe lip or axial spring loaded lip
  • Specially formulated elastomer and bonding agents
  • R-Safe & spring loaded axial dirt lips

Benefits
  • Superior grease retention for the life of the bearing
  • Strong bond and resistance to Ethylene Glycol
  • Excellent contamination protection
SKF logo