Electric Motor Condition Monitoring

Second only to motor bearing failures, electrical shorts account for more than a third of all industrial motor failures. This is primarily due to degradation of the insulation in motors that prevents the electrical system inside a motor from shorting, or grounding out. Electrical testing of motors improves decision-making in the maintenance of motors and the rotating equipment they drive. It can help reduce costs as part of predictive maintenance (PdM) programs, by reducing cost of unplanned downtime and extending the service lives of critical motors.

Gain further insights about electric motor condition monitoring