Predictive Maintenance of Mechanical Failures

Predictive maintenance of mechanical failures, using electrical measurements for instantaneous torque


Historically, vibration analysis technology was the only means available to assess many mechanical failures in the field. However, there are conditions in which it is physically impossible to reach proximity to the system in question, being either motor or the driven load. Using examples from recent field experiences, the technology’s approach and the breakthrough value of the instantaneous torque signal will be evaluated diagnosing several case studies in the field.

Please fill out the form below to Download SKF’s official Preventive Maintenance Program guide for Free.