Kormarine 2015 – International Marine, Shipbuilding, Offshore

October 20 - 23, 2015

Location: Busan, Korea
Venue: Bexco (Busan Exhibition & Convention Center), U-dong, Busan, Korea
Booth number: Booth in the German Pavilion / Booth number not fixed.

Website: http://www.kormarine.com/2015

Short description of event:
Kormarine is an international marine exhibition in Busan. There, a variety of exhibitors will present diesel engines, pumps, compressors, valves, navigation systems and communications, as well as ferries, boats and ships. In addition, numerous seminars and workshops, focusing on current industry topics are held. It is the leading trade fair of its kind in Asia.

Short description of SKF’s part of the event:
SKF Marine will be presenting its complete product portfolio at the Kormarine 2015 trade show. Bearings, couplings, lubrication systems and the SIMPLEX-COMPACT seal range will be displayed, as well as oily water separators and stabilizers Also on show there are supplementary services such as condition monitoring solutions and special services like alignment and on-site machining.

SKF logo