Technology in motor racing

Additional value for industrial and automotive markets

Racing Evocative Image_Green Racing Car
Pursuing excellence in technology, SKF is active in the motorsport industry and invests in the advanced development which generates additional value to the industrial and automotive markets.

In 2011, the technical partnership with the Scuderia Ferrari team was renewed. This represents the longest technical cooperation ever in F1 history. SKF provides several components in this field for the most demanding engineering applications, such as low friction sealing materials, hybrid bearings and solutions for the Kinetic Energy Recovery System (KERS).

Find more about SKF offers in the racing industry.
SKF logo