Cages

SKF double row deep groove ball bearings are fitted with two snap-type, ball centred glass fibre reinforced PA66 cages (designation suffix TN9, fig. 1).
The lubricants generally used for rolling bearings do not have a detrimental effect on cage properties. However, some synthetic oils and greases with a synthetic oil base and lubricants containing EP additives, when used at high temperatures, can have a detrimental effect on polyamide cages. For additional information about the suitability of cages, refer to Cages and Cage materials.
SKF logo