Sealing solutions

FNL flanged housings are equipped with low-friction, double-lip grease seals (fig. 1). Table 1 provides an overview of the characteristics and suitability of the sealing solution. This information should be used as a guideline and does not substitute for testing a seal in its application.

Seals are supplied with the housing. If additional seals are needed, they can be ordered separately. They are identified by the designation prefix TFL followed by a number indicating the size, e.g. TFL 511.

SKF logo