Matched bearings

SKF can supply matched bearings. To match bearings, SKF combines bearings so that the difference in cross-section height lies within a very small tolerance range. This reduced tolerance range is a precondition for equal load sharing between the bearings.
Matched bearings are identified by a designation suffix:
  • DR for a set of two bearings
  • TR for a set of three bearings
  • QR for a set of four bearings
For additional information, contact the SKF application engineering service.
SKF logo