Our competences

Application expertise
SKF has over 100 years of experience of rotating equipment, and how machine components are interrelated, in every major industry worldwide. SKF Engineering Consultancy Services works on a daily basis with a big variety of customer applications and company sizes, ranging from industrial to automotive industries and aerospace to racing industries. All SKF Engineering Consultancy Services team members are experienced engineers, many with a background in application engineering.Calculations and computer simulations
To help customers compare alternative designs, verifying existing and new machines, identifying root causes of failing machines, good simulation tools are essential. Using both SKF propriety tools as well as commercial tools we can verify if a bearing arrangement fulfills the functional requirements, for example that it has been dimensioned correctly and that reliable operation is obtained based on the actual operating conditions.Lubrication engineering and tribology
SKF Engineering Consultancy Services has been involved in lubrication advises for complicated applications such as marine propulsion, vacuum pumps, and off-shore wind turbines. Other typical activities are lubrication analysis of tested or failing applications, checking for the condition of the used lubricants as well as chemical elements and contaminants in lubricants.Material analysis
SKF Engineering Consultancy Services can analyze the operating and lubrication conditions of bearings; during testing, in production or after failure. Often visual inspection is enough to draw conclusions and to make recommendations for required changes and improvements. When needed we can also use more advanced techniques to predict remaining life with X-Ray diffraction, or evaluate bearing surface conditions and elements using Scanning Electron Microscopes.Design for Six Sigma
SKF Engineering Consultancy Services applies the Design for Six Sigma methodology. This is a structured way of working, using proven quality tools to ensure design optimization and robustness.Typical activities are sensitivity studies by means of Design of Experiments, which let us identify parameters that offer the biggest improvement potential in a design, leading to optimized performance and reliability.
Take a closer look at knowledge engineering at work
-
Deep sea production equipment designed for optimal service life
SKF Engineering Consultancy Services helps major oil and gas producer achieve increased service life of deep sea production equipment.
-
Increasing wind turbine service life
SKF Engineering Consultancy Services helps turbine manufacturer design for a potential 20-year product service life
-
Optimized power train design
SKF Engineering Consultancy Services helps increase drive train efficiency and reduce C02 emissions