Learning and development

Catalyst to self-empowerment

SKF has a fairly high retention rate and it is not unusual to meet employees, staff and workers alike, that have been with the company for decades. Many view the company as part of their family where their grandparents, parents, siblings or spouse are working in the same company.

One of the reasons this is so may be the fact we offer personal learning and development opportunities to our employees. A concrete example is SKF’s Individual Development Plan (IDP) - an entitlement for all our employees.

The implementation of IDP's and performance reviews are followed up by the company wide employee survey as part of the Working Climate Process. The next is due in 2017.

Latest results
  • 69% (60) of the Group’s 45,000 employees have had a performance review within the last 12 months,
  • 60% (54) consider that they have an individual development plan in agreement with their immediate manager.

IDP serves as the basis for skills improvement and training recommendations. Our training programmes encompass both professional skills such as sales and marketing, leadership skills, and personal skills such as negotiation or time management.

Making learning more accessible for our employees is also the driver for creating the SKF College, with campuses in Europe, Asia and North and South America. SKF's global curriculum are locally adapted and provided in local languages at the campuses, thus reducing the need for long distance traveling and being away from work and family. 

SKF also offers various talent management programme to help develop future leaders in the company. For more information on learning and development at SKF, please visit our Career section (below).
SKF logo