Attention Microlog Analyzer customers on firmware v3.07 or earlier
(only applies to models CMXA 45, CMXA 48, CMXA 75, and CMXA 80)
In 2013, SKF announced the availability of major firmware update v4.0, compatible with active Microlog Analyzer products. One of the more obvious and perhaps significant changes introduced in v4.0 was a completely re-designed, more intuitive user interface - which meant even the long-time Microlog Analyzer users had to become familiar again with its look and feel (and functionality changes). As one might expect, a slight learning curve was normal - especially considering the full list of changes included in the release. Having said that, SKF highly recommends that any Microlog Analyzer users on v3.07 or earlier wishing to upgrade, click HERE.first to review each change n detail and prepare as needed.
Note: Microlog Analyzers with serial numbers before 1210XXX will require a hardware modification in order to use 3-channel plus tacho support for the Run Up Coast Down and Recorder modules. The hardware modification is free of charge for units with PSP coverage. Otherwise without coverage, this modification would be considered a normal billable repair.