Europort – Exhibition for maritime technology

November 03 - 06, 2015

Location: Rotterdam, The Netherlands

Venue: Ahoy Rotterdam
Booth number: 1510

Event website: Europort - exhibition for maritime technology

Short description of event:
Established as one of the world's leading maritime exhibitions, attracting visitor numbers of about 30,000 maritime professionals from 84 countries, Europort is a must attend for anyone who wants to stay ahead in the international maritime market. Bringing together all sectors of the maritime chain under one roof, Europort is unrivalled as a platform to showcase innovation and connect to the wider maritime community. For the 2015 edition a number of 1,100 exhibitors and 16 country pavilions are expected.


Short description of SKF’s part in the event:
SKF Marine will be presenting its complete product portfolio at the Europort trade show. Bearings, couplings, lubrication systems and the SIMPLEX-COMPACT seal range will be displayed, as well as oily water separators and stabilizers. Also on show there are services such as condition monitoring solutions and mechanical services like alignment, on-site machining, 3D measurements  and chocking. Further ShaftDesigner software for shaft alignment and vibration calculations will be demonstrated as well as the SKF Vibracon product range.

SKF logo