SKF in Malaysia

SKF presence in Malaysia started off with the incorporation of SKF Malaysia Sdn. Bhd, a sales and service company in 1973 located in Kuala Lumpur.

Subsequently in 1991, SKF Bearing Industries (Malaysia) Sdn. Bhd., a manufacturing plant was set up in Nilai, Negeri Sembilan. Since then, both business units have grown exponentially with more than 600 employees in both locations. The manufacturing facility in Nilai is one of SKF’s most modern and technologically advanced manufacturing plant. In line with SKF global quality standards, all manufacturing and quality control processes are fully automated and equipped with state-of-the-art machinery for producing the latest generation of bearings.

The sales and service establishment in Kuala Lumpur has been successfully meeting market demands of the industrial and automotive segments throughout Malaysia via the establishment of a strong network of distributors and dealers; besides providing application and technical services to end-users and OEM customers directly.

Product Assortment

SKF Nilai manufactures and supplies Deep Groove Ball Bearings, Self-Aligning Ball Bearings and Spherical Roller Bearings to renowned multinational customers across Asia, Europe and Americas.
These bearings are mainly used in precision applications such as electric motors, industrial gearboxes, material handling, textile, food & beverage, cars, trucks and many others.

Nilai Product Assortment

SKF Nilai International Certification

1997:    ISO 9002
1998:    ISO 14001
1999:    QS 9000
2003:    ISO/TS 16949
2003:    OHSAS 18001
2014:    ISO 50001
2018:    IATF 16949
SKF logo