MEB 95

MEB 95
The development of the MEB 95 is a step forward in the area of vibration testing. The MEB 95 is one of the latest generation of vibration testing electronics which can be used for in- and offline vibration measurements.

The MEB 95 is actually an industrial PC combined with some specific hardware components. A high-precision Data Acquisition Board (A/D card) is used to read in vibration signals. This board also handles the loudspeaker output.

MEB 95

SKF logo