Crank web deflections (crankshafts)

Align for optimal performance

It is important to have the alignment of crank webs checked regularly. Even when the crank webs are aligned correctly during installation, the alignment can change over time due to deflections in the machine base, worn support structures or changes in bolt tension.

SKF has extensive experience in measuring crank web deflections - even in the most challenging situations, anywhere in the world.

SKF logo