The advantages and disadvantages of signal averaging

Facts
Date: 2016
Price:$59
Language: English
Microlog

Summary

The nature of sound and vibration is that it is variable and comes in many different forms. Simple categories include; deterministic, periodic, stationary, random, non-stationary &
 transient. One method to separate periodic signals from random signals is to use averaging which, on the whole, works extremely well. But there are special cases where averaging doesn't work so well and careful consideration needs to be given to the appropriate approach.
Enter promo code
SKF logo