Transport and distribution

Goods transport related to SKF’s operations generates roughly more than 100,000 tonnes of CO2 emissions per year. Air freight stands for the largest proportion of the reported emissions despite the fact that the volumes transported by air are small. In 2011 59% of the reported transport emissions derived from air freight despite the fact it only carried 1% of the reported volume.

Target

30% reduction of CO2 emissions/tonne-kilometre for goods transport by 2016 compared to 2011.

Climate change targets across the value chain

SKF logo