Ordering information

SBD plummer (pillow) block housings and THD take-up housings are supplied with the appropriate covers, labyrinth rings and, if needed, adapter rings. End plates to secure a bearing on a cylindrical seat at the end of a shaft are not supplied with the housings. Bearings and adapter sleeves must be ordered separately.

Order example

Two SBD plummer block housings are required for two 22213 EK spherical roller bearings on adapter sleeves. One housing accommodates the non-locating bearing at the end of the shaft. The other housing accommodates the locating bearing and a through shaft.
The following items should be ordered:
  • 1 housing SBDD 2213 AL
  • 1 housing SBDD 2213 BF
SKF logo